デルタは、オープンフレーム医療用電源「MEPシリーズ」の最新ラインナップとして、MEP-600A24J BRAを発表しました。このモデルは、3" × 5"(7.62 × 1 ...
デルタは、医療用AC-DCアダプター「MEAシリーズ」の最新300Wモデル「MEA-300A24C HAA」を発売します。本モデルは24V出力を提供し、医療用画像診断装置、 ...
デルタは、屋外および産業用照明向けに高性能な電力を供給する、新開発の「EUCI BASICシリーズ」LEDドライバーを発売します。本シリーズはNFCによるワイヤレスプログラ ...
デルタは、ハイエンドDINレール電源「Force-GTシリーズ」の3相モデルに、新たに48Vモデルを追加しました。これにより、お客様の用途に応じたより幅広い出力電圧オプショ ...
デルタは、EUCO Arena SportシリーズLEDドライバーに、最新の1,400W出力モデルを追加し、製品ラインアップを拡充しました。EUCO-1400Wは、プロ ...
Delta adds the MEA-160A to its high performance medical adapter MEA Series, which deli ...
Delta has expanded its medical adapter MEA Series with 65 W models Class II double iso ...
Delta has announced the release of its latest driver from its cutting-edge high power ...
Delta introduces the new 2,000 W model for its IMA PLUS Series AC/DC power supply, whi ...
Delta proudly announced the addition of 150W and 600W models to its panel mount powe ...
Delta introduces the latest DIN rail power supply Chrome II Series. The Chrome II Se ...
Delta, a global leading provider of power and thermal management solutions, today announce ...
Delta introduces the LED Driver USCI LITE and USC4 LITE series in 200W/100W/55W models. Th ...
Delta expands its panel mount power supply PMR series by releasing the new 240 W model, ...
Delta expands the MEB Series with the launch of the 1,500 W medical grade enclosed power ...