Delta Presents Latest Industrial Power Supplies at IIFES in Japan


Tokyo, Jan. 26-28, 2022 – Delta has just presented its latest industrial power supplies together with industrial automation solutions at the Innovative Industry Fair for E x E Solution (IIFEE) in Japan. IIFES is one of Japan’s major industrial events, with a focus on cutting-edge technologies and information for the electrical and measurement industry.

During the 3-day exhibition, many visitors came to Delta’s booth to see newest industrial power supply series including:

  • DIN Rail Power Supplies:
    - New FORCE GT Series (12 - 48 V output) is slim and highly efficient, and is the 1st 80 PLUS Platinum certified industrial DIN rail power supply series in the world.
    - LYTE II Series is designed with full functions for general industrial applications.
  • Panel Mount Power Supplies:
    - PMT2 Series has a low profile design, and offers output voltages ranging from 12 V to 48 V and is suitable for general industrial applications
    - PMC Series features 24 V, 600 W power and is compliant with Japan PSE (DENAN). It is 20% smaller than the previous model with a high efficiency > 92% @230 Vac.
  • Open Frame Power Supply: PJB Series provides 24 V power with a power boost of 200% for 10 seconds and low inrush current.


Find out more about Delta’s offerings, sales and service support and upcoming events, please visit www.DeltaPSU.com





関連ニュース

デルタ、SPS Nuremberg 2024にて業界をリードする電源ソリューションを披露し、製造効率を向上

ドイツ、ニュルンベルク - 2024年11月12日〜14日 - 電力管理およびIoTベースのスマートグリーンソリューションを提供するグローバルリーダーであるデルタは、「SPS Nu ...

詳細

Delta Joins CIIF 2018 to Showcase Industrial Power Supply and Power Management

Shanghai, China, Sep 19-23, 2018 – Delta joined China International Industry Fair (CIIF) 2 ...

詳細

Delta Showcases Industrial Power Supplies Force-GT Series at METALEX Vietnam Exhibition 2022

Ho Chi Minh, Vietnam, October 6th – 8th, 2022 - Delta, a world-class provider of power man ...

詳細

メルマガ登録する

最新のイベント情報やニュースをお届けします

メルマガ登録する

最新のイベント情報やニュースをお届けします