Delta Introduced Medical Power Solutions and Industrial Power Supplies at MEDIX 2017 (Japan)


Tokyo, Japan, June 21-23, 2017 – Delta Electronics introduced medical power solutions and industrial power supplies at 8th Medical Device Development Expo (MEDIX) 2017, the exhibition which brings together latest technologies from around the world to design and manufacture medical devices.

In this exhibition, Delta showcased the new MEB-1K2 model which can provide up to 1,200W output power in a 5” x 8” form factor. With built-in intelligent fan speed control, MEB-1K2 integrates PMBus Rev 1.3 functionality and optional RS485. The MEB-1K2 provides the highest level of protection for BF type medical applications by meeting 2xMOPP standards.

Another new medical power supply showcased in the exhibition is the MEU-600C. This model offers 600W output power with high power density of 9.5W / inch3. The power supply comes with the same features as MEB-1K2. The MEU-600C incorporates a highly efficient convection cooling design to provide full power up to 50C without the need for an external fan.

To know more about the upcoming events, please visit http://www.deltapsu.com/events


Delta Introduced Medical Power Solutions and Industrial Power Supplies at MEDIX 2017 (Japan)



Various type of Delta's Medical Power Supplies and Industrial Power Supplies



Delta showcased the latest models at exhibition



From the left to right, Mr. Yangsun (Electrical Engineer), Mr. Ken (Sales of Delta Japan), Mr. Dennis (Product Manager of DELTA Taiwan), Mr. Osamu (Sales Manager of DELTA Japan), Mr. Kin (Sales of DELTA Japan), Mr. Jun (Sales of DELTA Japan)

関連ニュース

Delta Showcases Industrial Automation, Industrial Power Supply and LED Innovations at National Manufacturing Week 2018

Sydney, Australia, May 9-11, 2018– Delta Energy Systems Australia showcased its portfolio ...

詳細

Delta Presented Advanced Medical Power Supplies at CMEF Spring 2021

Shanghai, China, May 13 - 16, 2021 - Delta showcased various types of medical power suppli ...

詳細

Delta Showcases Cutting-Edge Medical Power Supplies at MEDICA 2023

Dusseldorf, Germany, November 13-16, 2023 – Delta, a global leader in power and thermal ma ...

詳細

メルマガ登録する

最新のイベント情報やニュースをお届けします

メルマガ登録する

最新のイベント情報やニュースをお届けします