MEB-500A24F AA & PMC-24V600W1RW Upgrade Notice



MEB-500A24F AA and PMC-24V600W1RW models have built-in Remote ON_OFF (INHIBIT) function, which can be used to enable or disable only the main output (24V). 

Between Remote On/Off and Remote On/Off GND Output Status
SW ON (Short) ON
SW OFF (Open) OFF (Standby mode)


For the convenience of users, Delta provides an external jumper to turn on 24V main output directly. Users do not need to order an external mating connector to turn on 24V main output.


As a result, the PMC-24V600W1SW (no remote on/off) model will be discontinued because this function is already implemented into the PMC-24V600W1RW model.


For more details, please refer to the latest specifications on DeltaPSU website.


Related News

Attention

Delta provides all information in the catalog and datasheets on an “AS IS” basis and does ...

Read More

Standard Industrial Power Supply Production Transfer From Wujiang to Dongguan China (2022-004)

As part of Delta’s long-term manufacturing strategy, Delta standard industrial power suppl ...

Read More

Product Change Notice: CliQ II Series 24V 240W 2-Phase and 48V 240W 1-Phase

Delta has updated the CliQ II DRP-24V240W2BN due to the end-of-life (EOL) status of certai ...

Read More

Subscribe to our newsletter

Be the first to hear about new events, news and products!

Subscribe to our newsletter

Be the first to hear about new events, news and products!