Why is Power Boost beneficial?

Power Boost (also known as Peak Power capability) is especially beneficial in applications with high inrush current or dynamic load conditions—such as system startup, inductive loads, or parallel DC/DC converters.


In these scenarios, the instantaneous current demand can exceed the rated output of a power supply unit (PSU). Without sufficient overload capability, the output voltage may dip, potentially triggering system resets, interrupting operations, or causing equipment downtime.


By providing short-duration reserve power, Power Boost enables the PSU to maintain stable output voltage during these transient events. This ensures reliable startup and continuous system operation without disruption.


Additionally, Power Boost helps system designers avoid oversizing the PSU solely to accommodate brief peak loads, resulting in a more cost-effective and space-efficient design.


For more information, see related FAQs:

Subscribe to our newsletter

Be the first to hear about new events, news and products!

Subscribe to our newsletter

Be the first to hear about new events, news and products!