Delta Presents Latest Industrial Power Supplies at IIFES in Japan


Tokyo, Jan. 26-28, 2022 – Delta has just presented its latest industrial power supplies together with industrial automation solutions at the Innovative Industry Fair for E x E Solution (IIFEE) in Japan. IIFES is one of Japan’s major industrial events, with a focus on cutting-edge technologies and information for the electrical and measurement industry.

During the 3-day exhibition, many visitors came to Delta’s booth to see newest industrial power supply series including:

  • DIN Rail Power Supplies:
    - New FORCE GT Series (12 - 48 V output) is slim and highly efficient, and is the 1st 80 PLUS Platinum certified industrial DIN rail power supply series in the world.
    - LYTE II Series is designed with full functions for general industrial applications.
  • Panel Mount Power Supplies:
    - PMT2 Series has a low profile design, and offers output voltages ranging from 12 V to 48 V and is suitable for general industrial applications
    - PMC Series features 24 V, 600 W power and is compliant with Japan PSE (DENAN). It is 20% smaller than the previous model with a high efficiency > 92% @230 Vac.
  • Open Frame Power Supply: PJB Series provides 24 V power with a power boost of 200% for 10 seconds and low inrush current.


Find out more about Delta’s offerings, sales and service support and upcoming events, please visit www.DeltaPSU.com





関連ニュース

Delta Showcased its Broad Portfolio of Smart Energy-efficient Solutions and System Integration Capabilities at Hannover Messe 2017

Hannover, Germany, Apr. 24-28, 2017 – Delta demonstrated its wide spectrum of energy-effic ...

詳細

Delta Presented the Latest Medical Power Supplies at CMEF 2017 (China)

Shanghai, China, May 15-18, 2017 – Delta Electronics participated in the 76th&nb ...

詳細

Delta Showcased its Industrial Power Supplies and Industrial Automation Solutions at Automex 2017 (Malaysia)

Kuala Lumpur, Malaysia, May 24-27, 2017 – Delta Electronics demonstrated its industrial po ...

詳細

メルマガ登録する

最新のイベント情報やニュースをお届けします

メルマガ登録する

最新のイベント情報やニュースをお届けします