CliQ II Redundancy Solutions




Delta Electronics adds two Redundancy Modules, DRR-20A and DRR-40A to its CliQ II series of DIN Rail power management products. They are compatible with both 24Vdc and 48Vdc power supplies, offering redundancy functionality. These modules can also be used for Parallel operation.


The Redundancy function ensures zero system down time for the customer when one of the power supply fails or is being disconnected unexpectedly. Under normal circumstances, both power supplies are each operating at approximately 50% load. When one fails, the other automatically takes over, thus providing 100% load, and ensures that the system continues running


The fault relay function alerts the user of any failure through potential free contacts. The LED lights on the Redundancy Modules also indicate the health of each individual power supply.







How to Install CliQ II 24Vdc Redundancy Module:


Step 1. 

Measure the output voltages at no load from Vin 1 to Com i.e. Voltage Vin 1 to Com and Voltage Vin  2 to Com of Redundancy module. If the voltages are not the same, follow Step 2. If same, skip to Step 3.


Step 2.
Adjust the output voltages, with the help of VR on the Power Supply front panel marked as ADJUST, to the same level. For example, if PSU 1 is measuring 24.15Vdc and PSU 2 is measuring 24.25Vdc, adjust the output voltage of one to be the same as the other.


Step 3.
Connect the PSU to the end system load and measure the output voltages from Vin 1 to Com i.e. Voltage Vin 1 to Com and Voltage Vin 2 to Com of Redundancy module. Ensure that the output voltages are the same even after the 2 Power Supplies are connected to load. If not, adjust them as described in Step 2. A difference of both PSU ± 25mV is acceptable.

*The Redundancy Modules can be used for all PMC 24V, CliQ 24V, CliQ II 24V and 48V models.

For more information or enquiries, please do not hesitate to contact your local Delta Electronics distributor or visit www.DeltaPSU.com.


関連ニュース

デルタ、パワフルな1,400W IoT対応モデルでEUCO Arena SportシリーズLEDドライバーを拡充

デルタは、EUCO Arena SportシリーズLEDドライバーに、最新の1,400W出力モデルを追加し、製品ラインアップを拡充しました。EUCO-1400Wは、プロ ...

詳細

CliQ II 3-Phase DIN Rail Power Supply Now Available with 480W Output Power

Delta Electronics extends the 3-phase models for its CliQ II DIN Rail Power Supply ...

詳細

メルマガ登録する

最新のイベント情報やニュースをお届けします

メルマガ登録する

最新のイベント情報やニュースをお届けします