Delta Showcases Industrial Power Supplies and Solutions at Manufacturing Expo 2023


Bangkok, Thailand, June 21-24, 2023 – Delta, a leading provider of power and thermal management solutions, showcased its portfolio of industrial power supplies and solutions at the Manufacturing Expo 2023 held at BITEC in Bangkok.


Among the highlighted products are DIN rail power supplies Force-GT Series and LYTE II Series. Both Series have ultra-slim form factors and wide operating temperature ranging from -30°C to 70°C, ensuring stable power delivery in various industrial applications. The Force-GT Series, which offers comprehensive 120 W to 960 W output power, has up to 95% power conversion efficiency to cut energy consumption.


Another focus is Delta's panel mount power supplies, including the PMR Series and PMT2 Series. Both Series are in compliance with the harmonic current IEC/EN 61000-3-2 standard and have sleek as well as low-profile designs, ensuring safety and sparing installing spaces, meeting the demands of modern industrial environments. In addition, the PMR Series has a built-in active PFC circuit to enhance its stability and efficiency.


Other highlights included Delta's UPS system consisting of the CliQ M DC-UPS and battery modules, along with the DIN rail power supply CliQ M Series, suitable for applications such as industrial robots, building automation systems, turnstiles, and packaging machines. On the exhibition site, Delta presented a UPS system live demo to illustrate the effectiveness of the production downtime reduction and grabbed the attention of attendees.


For more information about Delta's power supply technologies for manufacturers, please get in touch with our representatives or leave a message via the Contact Us form.









İlgili Haberler

Delta Showcases Smart & Sustainable Solutions at TEMCA M&E Thailand 2023

Pattaya, Thailand – August 18-19, 2023 – Delta, a leading provider of power management and ...

Daha Fazla

Delta Showcases Portfolio of Medical Power Supplies at CMEF Autumn 2019

Qingdao, China, October 19-22, 2019 –Delta joined the CMEF Autumn 2019 event to showcase v ...

Daha Fazla

Delta Showcased its Efficient Medical Power Supplies and Industrial Power Supplies at CMEF Autumn 2017 (China)

Kunming, China, Oct 29 - Nov 1, 2017 – Delta Electronics participated in China Internation ...

Daha Fazla

Bültenimize abone olun

Yeni etkinlikleri, haberleri ve ürünleri ilk duyan siz olun!

Bültenimize abone olun

Yeni etkinlikleri, haberleri ve ürünleri ilk duyan siz olun!