Delta Successfully Showcases Efficient Power Supply Solutions at INTEC 2024


Coimbatore, India – June 6-10, 2024 - Delta, a global leader in power management and smart manufacturing solutions, made a significant impact at INTEC 2024 by presenting an array of state-of-the-art solutions to meet the industrial automation and power demands. Among the showcased exhibits were several industrial power supplies renowned for their exceptional efficiency and reliability.


For DIN rail power supplies, Delta presented the LYTE II and Force-GT Series. The two Series greatly reduce no-load power consumption and have high efficiency to cut unnecessary power waste. Their conformal coating on PCBAs design ensure durability and resilience against dust and pollutants. In addition, both Series are certified to IEC 61010-1/2-201 for industrial application safety. Its wide temperature from -30°C to 70°C allows applications under harsh environments. The LYTE II Series features 120 W to 480 W output power to provide customers reliable products in a cost-effective way. Meanwhile, the Force-GT Series offers power outputs from 120 W to 960 W, ultra-slim design and up to 95% high efficiency, suitable for high-end industrial applications. These high-performance power supplies also feature built-in constant current circuitry and built-in DC OK relay to ensure safe operation.


Other exhibited industrial power supplies include panel mount power supplies PMR and PMT2 Series. Both Series can operate between -30°C to 70°C temperature range and have a compact 1U low-profile design, suitable for space-limited installations without compromising on performance. The PMT2 Series offers output power ranging from 35 W to 350 W while the PMR Series features 150 W to 600 W with built-in active PFC.


Delta also unveiled the latest DIN rail power supply Chrome II Series to the Indian market for the first time. This Series features 30 W to 100 W output power and complies to DOE VI energy efficiency standard with its lower no-load power consumption. It conforms to National Electrical Code (NEC) Class 2 and Limited Power Source (LPS) to ensure stability and safety across diverse environments.


Throughout the event, our experts engaged with numerous attendees, showcasing how our products enhance the efficiency and reliability of industrial operations. If you have any questions or specific requirements about Delta’s power supplies, please leave us a message via the contact form on our website.


Delta showcases cutting-edge industrial automation solutions at INTEC 2024


Delta experts introduce how our advanced SMPS solutions can meet customers' needs and elevate their operations


Delta's industrial solutions presents drew significant interest from many visitors at INTEC 2024


Delta presents industrial automation solutions to empower manufacturers to achieve higher levels of efficiency, accuracy, and sustainability

İlgili Haberler

Delta Presented the Latest Medical Power Supplies at CMEF 2017 (China)

Shanghai, China, May 15-18, 2017 – Delta Electronics participated in the 76th&nb ...

Daha Fazla

Delta Presents Industrial Power Supplies and Smart Manufacturing Solutions at VIMF2023

Bac Ninh, Vietnam, November 8-10, 2023 – Delta, a world-class provider of power management ...

Daha Fazla

Bültenimize abone olun

Yeni etkinlikleri, haberleri ve ürünleri ilk duyan siz olun!

Bültenimize abone olun

Yeni etkinlikleri, haberleri ve ürünleri ilk duyan siz olun!