2023 Motion Control Show


...
Oct 25 - 27 2023
...
Seoul, South Korea
...
10:00:00 – 17:00:00

Delta, a global leader in power management and thermal solutions, announced its participation in the 2023 Motion Control Show. This renowned event targets the theme of smart factory, semiconductor equipment, and machine automation. It will be held from October 25th to 27th at the COEX Convention & Exhibition Center in Seoul, South Korea.


With 5-decade development of cutting-edge power technologies, Delta will introduce its advanced power supplies to meet the industrial automation needs. Highlights include:


The Force-GT Series and LYTE II series feature an ultra-slim design, a wide -30°C to 70°C operating temperature range, and a -40°C cold. These power supplies also feature conformal coating on the PCBAs to protect against dust and pollutants, applicable to harsh industrial environments. The Force-GT Series offers a 120 W to 960 W wide output with up to 95% efficiency and the LYTE II series has a 120 W to 480 W output power range. These features allow both series to be applied in harsh industrial scenarios to ensure stability and reliability.


The PMR series and the PMT2 series are designed with a low profile to be installed in limited spaces. These power supplies conform to the harmonic current IEC/EN 61000-3-2 standard to ensure stable operation. The PMR series, in particular, features a built-in active PFC circuit to reduce unnecessary energy waste for industrial equipment.


The MEG-A Series allows users to flexibly configure and select from 2 ~ 60 VDC power output with top-of-the-line power density up to 27 W/inch3. The series provides up to 9-slot frames that are compatible with three types of power modules. It also features a universal AC input and an extensive -20°C to 70°C operating temperature, making it an ideal choice for enhancing manufacturing productivity.


Don’t miss the chance to visit Delta’s booth at the 2023 Motion Control Show and discover the state-of-the-art industrial power solutions.

 

Delta Booth No. : Hall C, Booth No. C515

Website:  https://www.motioncontrol.kr/main

Location: COEX, 513, Yeongdong-daero, Gangnam-gu, Seoul 06164 Republic of Korea

Gelecek Etkinlikler

Light and Building 2026

Come visit Delta at Light + Building in Frankfurt - the world’s leading trade fair for lig ...

Daha Fazla

ECR 2026

Delta will present its latest innovations in medical power supplies at ECR 2026 from March ...

Daha Fazla

Euroshop 2026