Delta Presented Advanced Medical Power Supplies at CMEF Spring 2021


Shanghai, China, May 13 - 16, 2021 - Delta showcased various types of medical power supplies at The China International Medical Equipment Fair, a gateway to the medical equipment and manufacturing industry in the Asian-Pacific region.


The highlighted exhibits at Delta’s booth included:

  • MEG series AC-DC Configurable Power Supplies: Up to 9 individual slots for 3 types of charging modules to provide 3,000 W output power. The power density reaches 27 W/inch³ up to 93% efficiency. With digital programmable control through PC GUI, the MEG Series allows easy parameter settings and monitoring. Smart fan-speed control and AC inlet option for global adaptability satisfies the needs of both medical and industrial applications. Configure your own power supply at Configurable Power Selector now!

  • MEU series Open Frame Power Supplies: The newest MEU 650 W type was revealed for the first time during the event. The MEU 650W is in a very small 4”x6” form factor and is certified with medical and Information Technology Equipment (ITE) standards. It is suitable for BF type medical equipment and general industrial equipment.

  • MEB series Enclosed Power Supplies: A 750 W power supply with a peak power boost feature up to 1,200 W. The MEB Series is suitable for BF type medical products with smart fan speed control.

To find out more about Delta’s offerings, sales and service support and upcoming events, please visit www.DeltaPSU.com


İlgili Haberler

Delta Showcases Smart Manufacturing Automation Solutions at Manufacturing Expo 2019

Bangkok, Thailand, June 19-22, 2019- Delta Electronics (Thailand) PCL. showcased its portf ...

Daha Fazla

Delta Showcases Industrial Automation, Industrial Power Supply and LED Innovations at National Manufacturing Week 2018

Sydney, Australia, May 9-11, 2018– Delta Energy Systems Australia showcased its portfolio ...

Daha Fazla

Delta Presented Smart Power Solutions at Taipei Int'l Industrial Automation Exhibition 2022

Taipei, August 24th-27th, 2022 – Delta, a world-class provider of power management and ind ...

Daha Fazla

Bültenimize abone olun

Yeni etkinlikleri, haberleri ve ürünleri ilk duyan siz olun!

Bültenimize abone olun

Yeni etkinlikleri, haberleri ve ürünleri ilk duyan siz olun!