CIIF 2023


...
Sep 19 - 23 2023
...
Shanghai, China
...
08:30:00 – 17:00:00

Delta, the global leader in power and thermal management solutions, will participate in the 23rd China International Industry Fair (or CIIF 2023), which features technological, intelligent, and sustainable manufacturing under the theme “Digital Economy & Industrial Decarbonization.” The event is scheduled to take place from September 19th to 23rd at the National Exhibition and Convention Center in Shanghai, China.


To echo CIIF’s theme, Delta will present energy-efficient and environmental power and automation solutions for low-carbon and sustainable manufacturing. The exhibited cutting-edge power supplies include:


  • DIN rail power supply Force-GT Series
    It is the world’s first DIN rail power supply that is certified with 80 PLUS Platinum for 115 V Industrial. The Series boasts a power efficiency of up to 95%, 120 W to 960 W power outputs and 12 V to 48 V voltage outputs. Its -30°C to 70°C wide operating temperature, -40°C cold start ensure stability and reliability under harsh environments. It also has conformal coating on the PCBAs to protect against dust and pollutants to enhance operation safety.The DC OK relay design allows the Series to provide real-time monitoring to prevent abnormalities.

  • DIN rail power supply LYTE II Series and panel mount power supply PMT2 series
    Both Series feature compact designs that optimize installation space and their low no-load power minimizes energy consumption. The two Series have a wide range power outputs with a 120 W to 480 W power outputs for the LYTE II Series and a 35 W to 350 W power outputs for the PMT2 Series. Both high-runner products can operate stably within a -30°C to 70°C temperature range and their -40°C cold start capability ensures reliable function under harsh environments.

Join us at CIIF 2023 to dig out Delta’s innovative solutions for building automation, factory automation, machine automation, renewable energy, and others.

 

Delta Booth No. : Hall 6.1, Booth No. D001


Website:  https://www.ciif-expo.com/home


Location: National Exhibition and Convention Center (Shanghai), No. 333 Songze Avenue, Qingpu District, Shanghai, China


Gelecek Etkinlikler

Light and Building 2026

Come visit Delta at Light + Building in Frankfurt - the world’s leading trade fair for lig ...

Daha Fazla

ECR 2026

Delta will present its latest innovations in medical power supplies at ECR 2026 from March ...

Daha Fazla

Euroshop 2026