PMT2 Series Upgrade Notice


PMT2 Series Upgrade Notice


PMT-xx2BA series upgrade according to new certification standards. Hereunder is the content:

  • Implement new safety standard IEC/EN 62368-1 due to IEC/EN 60950-1 and IEC/EN 60065 merge in 2020.
  • Enhance the lightning surge immunity from 2KV/1KV to 4KV/2KV to fulfill more field applications and requirements.
  • Additional safety marks EAC and KC are implemented on to product spec label.

It is being implemented into 6 existing models (refer to below table). All upcoming new models in PMT-xx2BA series will also meet the new standards. For more details, please refer to the latest specifications on DeltaPSU website (www.DeltaPSU.com).


Model List:

Model Upgrade Rev. Upgrade Date
PMT-12V50W2BA 02 2019.12
PMT-12V100W2BA 02 2019.12
PMT-12V150W2BA 02 2019.12
PMT-24V50W2BA 02 2019.12
PMT-24V100W2BA 02 2019.12
PMT-24V150W2BA 02 2019.12


Label Change:

Before After
PMT-24V50W2BA



PMT-24V100W2BA



PMT-24V150W2BA




Mechanical Change:

Before After
PMT-12V/24V50W2BA



PMT-12V/24V100W2BA



PMT-12V/24V150W2BA




Related News

Product change notice of firmware update by adding new features (PCN-23-004)

Delta Electronics, Inc. will update the firmware of the following models: EUCO-1K5140GLA, ...

Read More

Product Upgrade Notice: Improved Surge Immunity for the Force-GT Series 3-Phase Models

At Delta, we recognize that reliable power delivery is crucial, especially in green energy ...

Read More

Delta Industrial Power Supply Certificate Upgrade Notice

IEC/UL/EN 60950-1 safety standard will be replaced by IEC/UL/EN 62368-1 on December 20th, ...

Read More

Subscribe to our newsletter

Be the first to hear about new events, news and products!

Subscribe to our newsletter

Be the first to hear about new events, news and products!