MEB-500A24F AA & PMC-24V600W1RW Upgrade Notice



MEB-500A24F AA and PMC-24V600W1RW models have built-in Remote ON_OFF (INHIBIT) function, which can be used to enable or disable only the main output (24V). 

Between Remote On/Off and Remote On/Off GND Output Status
SW ON (Short) ON
SW OFF (Open) OFF (Standby mode)


For the convenience of users, Delta provides an external jumper to turn on 24V main output directly. Users do not need to order an external mating connector to turn on 24V main output.


As a result, the PMC-24V600W1SW (no remote on/off) model will be discontinued because this function is already implemented into the PMC-24V600W1RW model.


For more details, please refer to the latest specifications on DeltaPSU website.


Related News

PJ Series Product Upgrade Notice (PCN-23-005)

Due to the impact of global material and component shortages, Delta PJ series power suppli ...

Read More

Product Notice: Update to the CliQ M Series DC-UPS Modules Front Labels

To better serve our customers, the front labels on the CliQ M Series DC-UPS modules have b ...

Read More

Open Frame PJT-40W & MDS-040APS Series Product Upgrade Notice

In order to upgrade to the latest IEC 62368-1:2018 (Ed 3.0) standards, Delta will remove t ...

Read More

Subscribe to our newsletter

Be the first to hear about new events, news and products!

Subscribe to our newsletter

Be the first to hear about new events, news and products!